Part Number: MCT8316Z-Q1
I am using the MCT8316ZT-Q1 in my design and unsure of the grounding as discribed in the data sheet they referance AGND and PGND and in the routing layout example can't tell if these grounds are the same or isolated. From previous usage of TI motor drive devices the grounds are the same, are these ground the same or are they seperate and if the same sould they be connected at the parts thermal pad, all the cartoons for circuit implementation use the same grounding symbol throught the data document which is confusing, can you provide the correct grounding approch for using this device.
Thanks in advance