Part Number: DRV8353
Hi Teams,
Please help review the schematic of DRV8353, which includes three half bridge driver circuits,
In addition, the motor voltage is 48V, the rated current is 24A, the Iq/A is 33.94A, and the peak current is approximately 100A. May I ask if the values of R65 sampling resistor (resistance and power), R66, and R67 in the following figure are acceptable? How much do we need to change if it's not possible?