This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8811 evm code example

Other Parts Discussed in Thread: DRV8811, DRV8811EVM

Hi,

  excuse me i'm new to texas instrument IDE, i've found in DRV8811 evaluation board page (http://www.ti.com/tool/drv8811evm )  a sample firmware project for DRV8811EVM but i cannot open it With CCS 5 as there's not any configuration file project. By opening the code i see it seems to be done with iar embedded workbench but this kind of project configuration fille misses too. As to you Do i only need to add each project files manually to a new project?

thanks a lot, Mario

  • Hi Mario,

    Yes, the MSP430 code included with the DRV8811EVM was compiled with IAR. However, it can be easily added into a CCS project and compile from within. We do not pack source code with configuration files as it is easier to just add into a project of your own choosing. Some of these EVM's source code can be compiled with the Kick Start but if we include the "non Kick Start" project structure, it will cause problems anyway. Hope the info helps!

    Best regards,

    Jose Quinones