I'm converting the demo SW sensored BLDC DRV8312 so that it can used for the DRV8301. Until now I haven't succeed to make the buildlevel 4 work as expected.
Do you have at TI already a demo SW sensored BLDC for the DRV8301?
Best regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm converting the demo SW sensored BLDC DRV8312 so that it can used for the DRV8301. Until now I haven't succeed to make the buildlevel 4 work as expected.
Do you have at TI already a demo SW sensored BLDC for the DRV8301?
Best regards,
Frank,
See attached for DRV8301 + F28035 + Sensored. Here is the readme
DRV8301 - Sensored BLDC
2011-12-12
To compile correctly the BLDC_int folder can reside somewhere like
C:\ti\controlSUITE\development_kits\drv8301_dev (new folder)
Note that there is a bunch of non-used and mis-named code; this was built up from an InstaSPIN-BLDC project for a customer sensored demo in a day…it works, but it’s not something we would want to publish.
Instructions for demo:
Make sure:
#define BUILDLEVEL LEVEL7
in BLDC_Int-Settings.h
Make sure project/active build config is: F2803x_DRV8301_RAM
Build and load program to controlcard.
Enable Real-time mode
Run
Set watch window to continous refresh
Add to watch window:
EnableFlag -- Set this to 1 to get motor control started
BackTicker -- This will increment to let you know the program is running
hallCommutateFlag -- Set this to 1 to change from force-commutate to speed-control
SpeedRef -- This is the target speed (in normalized to speed of 5000rpm)
(speed1).Speed -- This is the speed reading (from the speed macro, in nomrmalized pu)
(speed1).SpeedRpm -- This is the speed reading (in RPM)
These speeds are for a custom motor, but very similar to the NEMA17 BLDC
Speed (RPM) Speed (pu)
1200 0.24
1800 0.36
2500 0.50
2700 0.54
3300 0.66