This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV 8312 C2 Kit Port pin connections

Other Parts Discussed in Thread: DRV8312

Dear all,

There is a jumper J5 available in the baseboard of the DRV8312 C2 kit, which I think can be used as external port pins.

However, as I looked into the datasheet of DRV8312 Baseboard, it shows only the odd numbered pins

being connected to the controlCARD slot. What happens to the even numbered pins?

Are they connected to the controlCARD as well? Are there are any GPIO pins in the J5 slot that I can use to

connect to the controlCARD slot? 

Any help is highly appreciated.

Thanks & Regards,

Vignesh.