Hi TI,
Can you inform if I can setup DRV8829 to run DCM, but only control it with ENBL and PHASE?
Can you inform if I can use external resistor to set up 100% current?
Regards,
Sam,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Sam,
Yes you can. The truth table is shown on page 6....Table 2.
For 100% chopping current, you would connect ALL of the Ix pins to V3P3OUT. Your chopping current would then be Ichop = Vref / 5 * Rsense. This is described on page 7 of the datasheet. Vref can be provided with a voltage divider from V3P3OUT and Rsense is chosen as an external resistor connected between ISEN pins and GND as shown in the functional block diagram.