This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8301: Power Control

Other Parts Discussed in Thread: DRV8301

Hi,

i want to use a DRV8301 for a BLDC (3Phase) application (The Power Level is up to a few kW).

I also want to control the power by a uC via PWM. Is it possible to control the Power Level by using a PWM module at the Power Source or 
should i set the PWM Signal directly on the Input Ports of the DRDRV8301 ? 

Thanks!