Hello, I bought this stepper motor:
http://www.sparkfun.com/products/10847 Wantai motor 57BYGH420
Datasheet: http://dlnmh9ip6v2uc.cloudfront.net/datasheets/Robotics/57BYGH420.PDF
Phase: 4
Voltage: 3V
Current: 2A/phase
Step: 1.8°
I've read that a motor can support more voltage to have more torque but current should be limited.
I was advice to use an IC because I could get micro stepping, instead using transistors, but I don't know which IC is more suitable for my motor.
Any idea which IT IC should I use with this motor??
Thanks a lot!
Eduardo.-