Hello,
I was reviewing the datasheets for the DRV8841 and the DRV8842 and I noticed that the logic for the current control inputs is opposite. I am looking to use the DRV8842 to actuate a solenoid and would like the maximum current. We previously used the DRV8841 and pulled the current pins low for max current, I want to make sure that in the next revision of the board I will need to tie the current control pins high on the drv8842 to get the maximum.
Thanks,
Chris