Greetings,
I have a design which uses a DRV8811. I need to add a second stepper motor and controller. The controller could be another DRV8811. But I am light on control bits.
Since I only have to run one motor at a time, I was wondering if I could share all of the control lines, except RESETn,This assumes I do not need to keep current in the windings of the idle motor.
I am full stepping both motors. The main wrinkle I see is that applying RESETn forces the indexer to home. If the indexer was not home when RESETn is applied, will the motor move when it is removed?
Any other gotchas?
I think I could also switch to a DRV8821 dial controller, but since it has 2 complete sets of control lines, I think the same considerations would apply.
Gerry Belanger