hello frndz.....
i m working on arduino board...
i have made it prototype
when i connect a motor and give an input motor does not rotate...and when i increase the current it starts rotating without any input...
what i measure is that when motor not connected..
voltage on pin 6 and 9 is 3.03 but when i connect the motor voltage on pin 6 becomes 2.46v and on pin9-1.91v...
and i also measure on original arduino board ,after connecting the motor voltage on pin6 and 9 remains same...
i also put an match pair resistors on these two pins but the situation is same...