Hello,
I would like to drive two DC motors that each use 24 Volts an about 1 A when working. The DRV8843 seems to be applicable to this use case, correct?
When i supply 5 Volts to either xIN1 or xIN2 inputs the expected outputs at xOUT1/xOUT2 should be at 24 Volts - correct?
The problem is that my setup doesnt work. When measuring the voltage between xOUT1 and xOUT2 without the motor connected i get about 6.3 V. When connecting the motor, nothing happens. Any suggestions about what im doing wrong? Ive wired VMA, VMB, SLEEP and RESET to +24 V and the inputs xIN1/2 are wired to switchable +5V. GND is connected and CP1 and CP2 are connected to capacitors according to the datasheet. To my best knowledge it should work, but apparently i forgot something. Any help?