Other Parts Discussed in Thread: DRV8843
Hello,
I am using the DRV8843 for controlling two DC motors simultaniously. The motors consume 0.1mA with no charge, each one.
When testing the driver just with a simple PWM, the motors consumptions are OK, but when we aplly a proportional speed control to the motors, they consume 0.5mA each, with no charge, which is unacceptable.
Is there any reason for that?
Beyond that, is there another way, instead of reseting the driver, for deal with the current limitation of 2.5A (that is less than the necessary for the motor to start running)?
Thanks