I have a question of DRV8412 EVM/
Our customer want to check the unusual condition.
1. GVDD=12V, PVDD=5V
2. Ta=80deg.C
3. PWM_C=0V, PWM_D=3.3V, M1,2,3=Low
4. 1.1ohms between OUTC and OUTD intead of DC mortor
Is this condition severe? Is there the possibility of the crack of the package? The Crack has occured with this condion in the customer evaluation.
Best regards,
Atsushi Yamauchi