Hi Everybody.
I just started drive an DC motor with DRV8842 and' i'm seeing strange, strange things. I already tried many things until two boards burned up.
Well, this unhappy event occurred when i was trying fix the lost torque problem.....
If I hold INx low and the other INx high, everything is just perfect (current, torque and etc..) but when i put pwm in one of the inputs.. for example 95% Ton and 05% Toff and hold the other input low, i get a torque about 10% of the one in the first case.
Any ideas??
Ps.: sorry about my english..
Thanks.