Other Parts Discussed in Thread: DRV2603EVM-CT, MSP430G2553, DRV2603
Hello,
I am having two problems with the DRV2603EVM-CT:
1) I am unable to switch to the binary mode outlined in the User Guide. I hold the "*" button down for more than 3 seconds, but it has no reaction to this.
2) I have downloaded the source code for the EVM, and have made slight modifications to it. I am trying to flash the program onto the MSP430G2553 using an eZ430-F2013. Using the FET-Pro40 (FET MSP430 Flash Programmer) - Elprotronic Inc. When I click on "Verify Security Fuse" it succeeds. However when I click "ERASE FLASH" it fails.
I would appreciate any help in this matter and would be happy to provide any additional information needed to help solve it.
Thanks,
Stuart