Hello, I am designing a board with several drv8301 and for one of them i only need to drive 2 half bridges.
What should I do with the unused pins ?
-----------------------------------------------------------------------------------------------------------------------------------------------.
For the pins of the buck :
I have only connected EN_BUCK to ground and the others (RT_CLK, COMP, VSENSE, SS_TR, PVDD2, BST_BK, PH)) are unconnected.
Is it correct ?
------------------------------------------------------------------------------------------------------------------------------------------------
For the pin of the unused half bridge :
I have pull down to ground INL_A and INH_A.
Is the capacitor between BST_A and SH_A still neccessary?
Can I put SH_A and SL_A to ground ?
Can I let GH_A, GL_A, unconnected ?
Best regards