Hi Sir / Madam ,
This vengat here from Avnet , one of our customer selected the DRV8432 for their product . Each product will have 3 BLDC Motor to driver it . Product is getting powered by Solar - Battery . In data sheet PVDD supply of DRV8432 - go up to to 52V. They are using a motor of 12V/5A(Peak)and 12/3A (continuous). customer want to give 12 V for VDD & PVDD also will it work ? It will create any layout issue ? what is bare minimum power DRV8432 will consume during no load condition (bcs want to put system in sleep mode to reduce the power consumption in night time ?
Rgds/
vengat.