This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question For DRV8805

Guru 19645 points
Other Parts Discussed in Thread: DRV8805

Please let me know three points below about DRV8805.

------------------------------------------------------------------------------------------------------------------------------------------
- What kind of function is nHOME?

- Although the 3.3V pull-up of the nHOME is Internal, is it satisfactory by No-Connect?

- Is there any application note about a setup and calculation of output current in addition to slva504?

------------------------------------------------------------------------------------------------------------------------------------------


Thank you for your consideration.

  • Hi Satoshi-san,

    nHOME is an output which tells the system whether the internal indexer is executing the HOME state as defined in the datasheet's logic lookup table.

    nHOME can be left disconnected if you do not wish to use this feature.

    Current throughout motor winding will be dependent on the winding and given byt its Ldi/dt. Once the inductor saturates (and hpoefully it doesn't), then current can be computed as VM/(Rwinding + RDSON). That is basically the largest current you should see on a per output basis.

    Hope the info helps. Best regards,

    Jose Quinones