This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8818 Motor Output Current Specification



What is the max current per channel (AOUT+, AOUT-, BOUT+, BOUT-)? I know the device is rated for 2.5A, but as I am designing the PCB I need to know some current specifications for each of the individual lines. I am assuming each line doesn’t need to carry the full 2.5A, but I am not sure of this and wanted to check what an appropriate current would be for which to design.
Let me know so I don't end up with excessively large traces and headers.
  • Kevin,

    The gerber files for the EVM are available on our website in a zip file.  You can open them and take the measurements.  If you are using the full RMS current in each winding, then the traces for AOUT-/+ and BOUT-/+ should all be sized to handle this current.