I am looking for suggestion regarding selection of appropriate stepper motor driver(bipolar). Following are the requirements specs of the stepper motor:
operating voltage | 2.33VDC |
Current/Phase | 2.6A |
Power Consumption | 14W |
Resistance/phase | 0.9 ohm |
- need to maintain the motor in the hold position for long hours (>6hrs.)
Also if possible would like to have a stall detection feature present in the IC. Will be driving the stepper motor driver using msp430 device.
Any help in this regards would be great!
-Yogesh