My question is in reference to Figure 13 (Schematic Example) on page 21 of the DRV8312/DRV8332 Datasheet (TI reference SLES256):
What is the voltage and current range for pins GND_A, GND_B, and GND_C ? They are shown in the schematic as connected to op-amp circuits that appear to be used for sending a voltage to the Analog-Digital Converter (ADC) module of a digital signal processor (DSP).
I want to do the same thing in my project. The ADC module input checks for a voltage of 0 (zero) volts, 0 volts <voltage<3 volts, and voltage >3 volts and converts this voltage into a digital value per the ADC datasheet. In order for me to analyse the circuit, I need to know the voltage and current at the GND_A, GND_B and GND_C pins.