We have ordered samples of DRV8818 from TI. One of our company's application require a stepper motor driver, for which we designed the attached schematics. We will only be using the step input, whereas other inputs are permanently fixed on the hardware.
The problem I am facing is that the stepper motor rotates but not smoothly. i.e. It rotates unevenly, as if any of the coil is not energized periodically! When I check the waveforms on the outputs, I get some unclear waves on every output. I have attached my schematics. I have used 555 Timer to generate clock signal and this clock (Square wave) goes to step input of the IC.
Please check my schematics and let me know the mistake I am making or the possible cause for my issue.