Hello,
I am trying to use the DRV8843 in my robot setup and unfortunately all my attempts are not successful at the moment.
Here is my setup:
1 CP1 -- capacitor in between 50V 0.01uF
2 CP2 /
3 VCP - connected through 0.1uF to VM (actually I am using 50V rated capacitor as I don't have 16V handy)
4 VMA - 10V (power supply)
5 AOUT1 - motor lead
6 ISENA - GND
7 AOUT2 - another motor lead
8 BOUT2 - N/C
9 ISENB - GND
10 BOUT1 - N/C
11 VMB - 10V (power supply)
12 AVREF - 3.3V (also tried N/C)
13 BVREF - 3.3V (also tried N/C)
14 GND - GND
15 V3P3OUT - N/C
16 nRESET - 3.3V
17 nSLEEP - 3.3V
18 nFAULT - N/C
19 DECAY - N/C (tried 3.3V)
20 AIN 2 - GND
21 AIN1 - 3.3V
22 BIN1 - N/C
23 BIN2 - N/C
24 AI0 - GND
25 AI1 - GND
26 BI0 - N/C
27 BI1 - N/C
28 GND - GND
If the motor is not connected I can see almost proper voltage between AOUT1 and AOUT2 (~8.8V). But as soon as I am connecting motor - voltage drops till 0V.
The motor when running just with power supply draws ~ 100mA.
The GND PPAD is not connected to the copper (I solder the IC to protoboard). Can it be the reason ?
I am seriously running out of ideas what can be wrong.
Regards,
Anton