Hi, I need to evaluate and drive a BLDC direct drive wasing machine motor on a rig similar to a washing machine to determine maximum torque, vibration and movement of the rig from around 30rpm up to 1600rpm and do not have the motor parameters.
The motor is very similar looking to that pictured on page 2 of the TI Motor and Drive Control Solutions Brochure.
Very impressed by the info on TI's new Instaspin and driver kits but as a mechanical engineer with very little electrical engineering knowledge I would be grateful of some advice in choosing the correct evaluation kit.