Hi,
We are using the DRV8601 and the current design is driving it with a PWM signal. Two questions:
1] Is there an applicaiton note that provides direction on PWM controls (e.g. frequency, duty cycle, etc.) to provide different haptic sensations/effects? FOr example how to drive to generate a "thump" or a "sweep" effectm to name a couple.
2] The Datasheet states - "The DRV8601 can accept a single-ended PWM source or single-ended DC control voltage and perform
single-ended to differential conversion." Is there an application note for driving the device with the "DC control voltage"?
Thanks.
-Doug