Hi
I am presently using TI DRV8821/DRV8823 motor driving module. the problem i am facing is unpredictability of the output at the motor output pin . I am using the DRV8823 MODULE application software where i am making the following settings
AENABLE MARK
APHASE MARK
ADECAY MARK
RESET MARK
SLEEPN MARK
when i am changing the reference voltage i.e VREFAB to 0 i sometime i got 12 volt and sometime 24 volt on the A+ AND A- PIN OF THE BOARD.
please help me out in configuring the board .