Hi...
Is it possible to reduce the internal amplification of the DRV8301 by placing additional serial resistors in front of SN and SP? According to DRV8301 pdf (SLOS719, page 13) the op amplification is set by a 5k serial resistor and 50k/100k/200k/400k in feedback loop resulting in 10x/20x/40x/80x.
Adding additional resistors in front of SN/SP of
a) e.g. 5k would lower the resulting amplification to 5x/10x/20x/80x.
b) e.g. 15k would lower the resulting amplification to 2.5x/5x/7.5x/10x.
Is that possible?
Gerd