Hello,
I was looking at page http://www.pololu.com/catalog/product/2133, and I have a couple of question related to the use of the driver.
For my application, I need to drive a stepping motor at 60RPM with a torque of 2.5Nm. I have selected a stepping motor that has a max permissible torque of 3Nm and the rated current per phase is 0.6A. The stepper motor is a NEMA 16 with a 14:1 planetary gearbox and so the step angle is 0.131degrees.
My question is how can I calculate what RPM the DRV8825 stepper motor driver can drive the stepper motor at?
I've read the TI datasheet for the DRV8825 which says that the maximum step frequency is 250kHz I assume this is for the highest micro-stepping resolution at 1/32 and with the maximum driver output current of 2.5A.
Is there a reference table or simple formula I can use to determine the maximum step frequency at lower micro-stepping resolutions and lower driver output currents?
Is the relationship between micro-stepping and torque linear? As I have read that the mirco-stepping reduces torque?