Hello
We are busy designing a new Driver board and would like to be able to choose between BLDC, Bipolar stepper motor and Brushed DC is it possible to use the DRV8432 for the brushless motor? even if we have to add some extra logic to the system, if this is possible do you have the IC's for this?
The DRV8332 only has the capability for BLDC right? or also Brushed DC.
Regards
Edwin