This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8801 VCP current?

Other Parts Discussed in Thread: DRV8801

I'm using the DRV8801 to drive a DC motor at 10V, max current 1.5 A, no PWM.
The motor is driving a gearbox with some load on it and we are testing the concept by driving the motor in a continuous cycle:
Start Clockwise --> Delay --> Stop/Break using slow decay mode. Then same cycle again but counter clockwise. Delay is 3 sec.
After some 200 000 cycles VCP capacitor just blew up in pieces.

Now I'm trying to find in the data sheets what minimum current rating I should have on the VCP capacitor - but I can't find any figures.

A hint would be very much appreciated.

Cheers,

Michel