Hello,
I recently completed a test that required control of eight BLDC motors (48V/5A/10k RPM) using eight DRV8301-HC-C2-KIT eval boards running lightly modified Instaspin software and a Stellaris Launchpad to control them all over SPI. This worked well, but required a huge box, so the next stage of the project will require a custom board or boards to minimize the package volume. For the power drive section, I am planning to closely copy the DRV8301-HC-C2-KIT schematic with the layout modified to minimize PCB area.
My question is how many motors could be controlled with a single F28035 controlCARD as included with the eval kits that I have?
I suspect that all eight DRV8301/motor combinations controlled by one processor would not be possible, based on reading the spry135.pdf whitepaper, which seemed to indicate not a lot of extra headroom running two motors, but that app note is for FOC control, which I imagine is more processor intensive than the Instaspin trapezoidal drive? Also I don't need the PFC described in that app note.
Would there be a better processor choice?
Thanks for any help you can provide.
Pete