So after following the "Read me first" pdf several times, I cannot get the instant spin to work. The board is configured properly, the drivers are installed and showing up in device manager, and I have installed the GUI Composer Runtime, Motorware, and Motorware GUI all in the right directories. After I open the launcher.exe, the splash window appears, then a blank window opens and nothing happens beyond that. Alls that is in the window is a dropdown and exit option, completely blank. Running windows 7.