Other Parts Discussed in Thread: DRV8312, INSTASPIN-BLDC
Hi, I'm using the DRV8312 Piccolo kit. Investigations with the kit motor went fine but when I switched to a Faulhaber 3564 motor I noticed a behavior I can't explain. The speed seems to be limited to around 7500 rpm even though I've set the base frequency to 333 Hz (4 poles) which would give me 10000 rpm max. I also changed the pwm frequency to 40k due to the low inductance of the motor. Do anyone have any advice to give?
Br, Johan