HI,,I am using the 12v,1200 rpm motor for my quad rotor ,,is drv10963 ic is good for the application of the bldc motor to run at its full speed ...because driver is about 5 v.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI,,I am using the 12v,1200 rpm motor for my quad rotor ,,is drv10963 ic is good for the application of the bldc motor to run at its full speed ...because driver is about 5 v.
Hello Jitu,
Welcome to the Forum!
The DRV10963 as you stated is only for 5.5V and unless you are only supplying 5V, then the DRV11873 : 12-V, 3-Phase Sensor-Less BLDC Motor Controller would probably be a better fit. It is rated up to 1.5A and can supply a 5V output.
This is just my suggestion, other options would depend on your exact motor specifications.
Thanks,