Dear friends,
I'm going to purchase The DRV8312-69M-KIT, An InstaSPIN-FOC and InstaSPIN-MOTION technology-based motor control evaluation kit, for spinning three-phase BLDC and PMSM motors.
The kit includes:
- BLDC/BLAC NEMA17 55W Motor
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear friends,
I'm going to purchase The DRV8312-69M-KIT, An InstaSPIN-FOC and InstaSPIN-MOTION technology-based motor control evaluation kit, for spinning three-phase BLDC and PMSM motors.
The kit includes:
Thnaks Ryan.
I want to control Sensored PMSM & BLDC Motor at very slow speed (say 1 rpm) (with both torque & speed PI).
Is there any development kit available in TI which has;
1. kit includes sensored PMSM/BLDC Motor,
2. Insta-spin support,
3. MCU TMS320F2806x.
4. along with DRV series MOSFET driver.
Chinmay,
Not sure what your current/voltage requirement needs are for the driver, but the following kit meets your requirments.
http://www.ti.com/tool/drv8312-69m-kit
Chinmay,
For low voltage kits we currently don't offer any sensored examples for low speed. But we are working on some internally. They will use the Teknic motor (built in encoder)) that is currently included in the DRV8301-LS31-KIT. For the power stage we are using DRV8312 and DRV8301 kits today, but we have some new hardware that will be out this summer that is DRV8302 based with NexFETs.
We also have a slick mounting system to couple two of the Teknic motors so that one can be used as an active dyno while you test your control on the other.
All the SW will be based on InstaSPIN-FOC and InstaSPIN-MOTION (-MOTION anytime we do sensored speed control).
Dear TI team,
Recently I bought this motor driver kit. I am trying to understand how to change the programm, kindly let me know what additional hard ware / soft ware tools are required to change the existing programm.
Also please send me the path to down load some sample test programms for PMSM sensorless control based on FOC.
http://www.ti.com/tool/drv8312-69m-kit
Thanks in advance for you help.
RK.
Dear Rick
Thanks for your collaboration. The information has been very useful.
Best regards,
Anderson