Other Parts Discussed in Thread: DRV8302, CONTROLSUITE, DRV8301, TPS54160
Dear Friends,
I'm going to design schematic for PMSM Motor Control project with using DRV8302.
I've read datasheet of DRV8302. Is there any application notes/material available for DRV8302?
I want to use Built-in Buck converter to power MCU & other logic of my design.
from datasheet, pin # 11, 12, 50-51, 55 connection details are not be cleared, also how to get 3.3V & 5V (for MCU & Logic) from buck converter is not understood clearly.