Dear Texas Instruments
I have implemented the DRV8800 into my design, while not using it as a motor driver, rather as a current protection and status feedback mechanism. The protection mechanism will protect my output interface if overloaded or shorten. I will by this have the output always on, with an expected current of typ. 100mA and a voltage of about 12V. I am using a switching controller, opening and closing MOSFETs, at the output of the motor driver, turning on and off the output sourced from the motor driver.
When using the current overload protection mechanism in the motor driver, it is stated in the data-sheet a shut-down time of typically 1.2ms. What I am having challenge in finding, is the information of the time from a fault is loaded on the output, to the motor driver actually is shutting down the output. If I have a small pulse (low energy) on the MOSFETs on the outside of the motor driver, will these spikes be enough to enable the over current protection mechanism...(?) I have a simulated average of 30mA, while simulating short spikes of about 6A. The simulation is of course a theoretical value, only giving a guide of the actual performance. I would also expect that the over current mechanism enable-timing will be dependent on the level of the current spikes. But lets say that the simulation is the actual levels in real life;
Is there any measurements or theoretical approximation of the time from the current fault is started, to the motor driver is defining it as a over current load situation, enabling the shutdown mechanism?
Sincerely
yours
K S