The DRV8301 has two current sense amplifiers which in the example circuit are shown to be used to amplify currents through resistors that have been placed in two of the three individual low side paths to ground (between the pull down resistor and ground in each case). In this configuration the system has visibility of the current 2/3 of the time but when current is going through the 3rd phase there is no way to read current. My question: why is the current not sensed in the path between the point where the three phases join together on the low side and ground? Is there an advantage to sensing two phases individually instead of the sum of all three? Also, why only two of the three phases - is this a cost reduction?
Thanks,
DMH