In the datasheet, under PWM input mode it reads "The DRV2605 drives the actuator continuously in this mode until the user sets the device into STANDBY mode".
I am unable to understand this logic. What is the point of having PWM if we have to set the device in STANDBY mode to turn off the pwm ? I get a continuous pwm pulse which is undesired. Should'nt this be operated based on duty cycle?