Other Parts Discussed in Thread: DRV8301
We use motors for two types of Remotely Piloted Aircraft System [RPAS] function:
- To power individually controllable ducted-fan / propeller propulsion units (4) using speed control (potentially up to 20,000RPM, but more likely initially up to 10-15,000RPM). The power/torque curves are defined by the fan / propeller power curves. (We also have dyno load systems that motors can plug into).
- To drive a camera payload gimbal in pan, tilt and roll using PWM position control.
I want to test a range of motors (11V up to 10A, 11V up to 20A, 22V up to 30A), can I do this using the one DRV8301 high current kit? My goal is to be able to develop high-efficiency controllers and confirm performance (volts, amps, watts & speed accuracy) against industry standard controllers (that don’t have variable gain control).
Having established the required performance, we will need to translate the test environment into a final controller design. I am therefore seeking to get a clear understanding of what TI components will be required to develop the final controller. Clearly there will need to be the right Piccolo MCU programmed with appropriate firmware and we will have, let’s say an 11V voltage rail. What other elements are required to develop a complete motor controller and what are the approximate masses of each individual component?
My final question relates to the selected Piccolo MCU. Can this MCU drive more than one motor (i.e. up to a maximum of 4 motors), with each motor being speed controlled individually or do I require four Piccolo MCU’s, one for each motor? If I can use one Piccolo to drive 4 motors, then clearly I can save weight.