This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Key Components for a TI InstaSPIN Derived Motor Controller

Other Parts Discussed in Thread: DRV8301, TMDSCNCD28069ISO, DRV8302

We want to develop a high-efficiency motor controller for an aerospace application (Remotely Piloted Aircraft Systems). Weight is therefore a critical consideration in the motor controller design. Once we have established an optimal design / software configuration using a TI DRV8301 and TI InstaSPIN MOTION, is there a core components list that outlines the critical components required to develop the final motor controller that we could use as the basis for determining the final controller weight.

 For example, we know that we will require a Piccolo F2806x for control of up to two motors and then there are the FETs. How many do we require per controller and what TI part numbers are we looking at for say an 11V, 10A controller, what part number for a TI motor pre-driver and voltage regulator? What other critical components do we require? The ideal would be to develop a spreadsheet where we would have a list of TI components, with their weights and depending upon voltage and max current draw could quickly establish the motor controller parts list, including number of components of the same type and the approx mass of the motor controller by total components selected. Any advice on this would be gratefully received.

  • Ashley,

    You would be best person to come-out with component lists because you are aware of complete system specifications for end equipment.  

    To get support on preparing the list you can check the Bill of Material (BOM) of TMDSCNCD28069ISO control card and DRV8301-HC-C2-Kit. These BOM will help you to find out voltage regulators, LDOs, isolation parts from TI portfolio. These BOMs are available in hardware development package of C2000 Control-suite which can be freely downloaded from:

    http://www.ti.com/tool/controlsuite

    You can also look into MOSFETs portfolio of Ti at http://www.ti.com/mosfet to select right part, because now TI offers highly efficient MOSFETs with low-rds and lower gate-charge in 30V/40V and 60V range which can meet your voltage and current requirement.

    Best Regards

    Milan

  • Hi Ashley,

    Of course, InstaSPIN implies you'd like to drive brushless DC motors (BLDC).  You'll need two DRV8301 devices or two DRV8302, as well as 12 power FETs to form 6 half-H bridges.  TI's latest power FETs are called NextFET.  The DRV devices feature an integrated buck converter that can power the microcontroller.

    Best regards,
    RE