Hello,
I have a DRV8313EVM hooked up to a power supply at +12 V and connected to a laptop through the micro USB cable supplied with the board. It has been configured as instructed in the User Guide. The connection seems stable, as the flashing light on the GUI alternates between green and light green. However, everytime I enable the motors by checking the "Enable Motor" option, the connection goes bad after about 7 flashes of the GUI heartbeat. It then proceeds to alternate between green and red, and eventually times out. I cannot restore connection until restarting the board. However, this always happens when the "Enable Motor" option is selected.
I've tried this under different scenarios, including using an input voltage of +24 V as specified in the manual. I've also experimented with changing the JP1 jumper connection. Originally I had it between pins 1-2, but also tried shorting pins 2-3. Is it a problem with communication between the DRV8313 and the MCU? Or is the board faulty? Thanks in advance for your help!
Regards,
Jake