This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

H-Bridge and its Driver ICs

Other Parts Discussed in Thread: DRV8711, DRV8301

Application     - DC Motor Drive Development

Motor Spec    - 24V DC, 20A, Permanent Magnet DC Motor

 

Required Solution 1: Integrated Motor Driver Solution (H-Bridge + Gate Controller on a single chip IC)

                                                - IC should support 30A current (best if without heat-sink)

                                                - On chip Short Circuit Protection, OV/UV Protection, Overshoot Protection ( If available will be better)

                                                - PWM control option ( Mandatory)

                                                - Min PWM frequency 10KHz

 

If Integrated solution is not available then we could go for separate H-Bridge & Gate Controller ICs

 

Required Solution 2: Motor Driver Solution (H-Bridge + Gate Controller both separate chips)

                                                - H-Bridge should support 30A current (best if without heat-sink)

                                                - Half-Bridge/Full Bridge Gate Driver Controller that should drive the H-Bridge

                                                - PWM control option ( Mandatory), min PWM freq 10KHz

 

Kindly, provide us with the suitable component part numbers meeting the above requirements. In case of further info, please feel free to contact

us on any of the numbers mentioned below

                               

Thanks,

Nitesh Agrawal

Tata Technologies Pvt Ltd –Pune

8087938383,

9975473016(Saurabh)

9665313970(Vinay)

Office – 020-66529851