Can the DRV2667 be configured to output 200VDC (no waveform) ?
Also, can 2 DRV2667's be put in series to output 400VDC?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
The DRV2667 is a differential output driver with a output voltage range from -100 to +100V. The integrated boost has a range from 0V to 105V. It is not possible to generate 200Vp from the DRV2667 alone. Unfortunately the DRV2667 cannot be placed in series either.
Thanks,
Brian