This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Motor controler

Other Parts Discussed in Thread: DRV8312, CONTROLSUITE, TMDSHVMTRINSPIN, TMS320F28069M, MOTORWARE, MOTORKITSCNCD69MISO, DRV8301

hello, I'm Albert Mendy, I am in training Keep in Motion and am working on a speed (frequency) for a three-phase permanent synchronous motor with  the following control modes: BLDC mode with Hall effect sensors,  sensorless vector control mode with position sensor (encoder or resolver)  with a communication will be CAN mode (DSP. ...). I search a development kit (hardware + software) to learn about controlling three-phase brushless motors. is the  DRV8312-C2-12-Kit OK for my need? if not, what can you propose?. the power for motor is 500W to 2000 W and the bus voltage is 48 V to 100 V.

thank.

Albert MENDY