When I need to measure the ambient temperature of ICs for simulation or derating purpose, where should I put the temperature sensors? I surpose the location should be the air above the component. But how much should be the gap between the case of the componet and the sensors? 5mm? 1cm? or can I just use the case temperature as the ambient temperature for these low power ICs?