Hi,
We are designing a DC motor drive (brushed, PWM controlled, 0.5hp, 19.5A peak). We have evaluated the DRV8432 as a perfect candidate for something a little less powerful than this particular motor (since DRV8432 has 14A max current), using the very useful DRV8432EVM.
We are using it in Parallel Full Bridge (PFB) mode. We see that even at a PWM frequency of 50% (generated and confirmed as correct, using an MSP430), the IC tends to reach it's over temperature warning (OTW) in about 7 minutes of constant operation (despite just 10A drawn, and 35 degrees ambient temperature), on the DRV8432EVM. Also, after about 15 minutes of this constant operation, the FAULT signal comes up.
1. While we try to debug this problem, is it acceptable to use power MOSFETs after the DRV8432 output pins in order to reduce the current load on the DRV? Of course, we would take care of the MOSFET specifications as per our load requirements. In this case, we could make do with a lower wattage DRV instead of the DRV8432.
2. What is the relationship between the PWM_A and PWM_B w.r.t. OUT_A and OUT_C in PFB mode? A diagram depicting the timing/signal relationship would be great. Any details on the braking, coasting, direction, etc would be most beneficial, as the same are missing from the device datasheet. We are OK with referring to another device's datasheet in case you confirm that the functionality/behaviour would be the same (except for the different current capacity, etc).
3. Are there any application notes using the integrated DRVs as pre-drivers?
4. How about using current and RPM sensing with these DRVs? We understand the principles, but any additional pointers would be helpful!
Thanks,
Anup