Hi,
I have a question about DRV8814 driver:
I´m using a 24V 0.9A dc motor with a start current of aprox. 4-5A and I´m having several problems starting motor because fault conditions set continuosly. I have read datasheet and other tech documents that tell about current control of the driver using a internal PWM control loop for avoid problems with start currents in DC motor.
I set the xVref to limit Ichop value of aprox 2.5A but I only get fault condition. If set the xI0:xI1 in way to decrease motor current, it´s worst...
Really driver control motor current ?, I think the only driver makes is to set the fault condition in function of xVref threshold voltage.
What´s the problem ?, Why driver no litmis motor current?
I hope your answer
Thanks in advance.
A. Garcia
I+D Engineer