Hello all,
I have designed a circuit around the DRV8834 PWP and have a prototype circuit card working. The microcontroller is issuing the proper commands in index mode to the stepper motors, STEP and DIR and I set AVREF and BVREF to 300 mA correctly. The nFAULT signal is toggling every 180 microseconds.(See attached). I used the POLOLU carrier for this chip to breadboard with (it worked great), and basically have built the circuit using that as the model on my prototype PCB. All the input signals to the DRV8834 are correct, except the stepper motor is not turning and the nFAULT line is toggling as mentioned. Any ideas? This is a very small board so I am limited in what I can do to correct this. I am interested in what may cause this. The chip is not hot, the current is limited, and the VM is okay (5 Vdc). This problem is on 2 of my prototype boards, I have 10, so I expect it is on all of them.
Thanks